AXIS#.IL.FB
Description
This parameter displays the measured actual q-component current reading.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
Arms |
|
Range |
± Axis peak current (AXIS#.IPEAK ) |
|
Default Value |
N/A |
|
Data Type |
Float |
|
See Also |
N/A |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.IL.FB |
500ah |
01h |
Signed32 |
- |
1000:1 |
Read only |
Yes |
|
AXIS2.IL.FB |
510ah |
01h |
Signed32 |
- |
1000:1 |
Read only |
Yes |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5803 |
1 |
5803 (0x16ab) |
AXIS1.IL.FB |
Signed32 |
Read Only |
Yes |
|
71339 |
2 |
5803 (0x16ab) |
AXIS2.IL.FB |
Signed32 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.IL.FB |
5803 |
Float |
Read Only |
- |